Number animation
A single animation
- BrowseName
- NumberAnimation
- SuperType
- Abstract animation(AbstractAnimation)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| From | From | Float | Start value of the range |
| To | To | Float | Final value of the range |
| Duration | Duration | Int32 | Duration of the animation in milliseconds |
| Interpolation | EasingCurve | Motion curve | Defines the interpolation distribution used for animating the value change |
| Target | Target | NodeId | Object that is used as target for the current method, event or action |
| Running | Running | Boolean | (Inherited from Abstract animation) |
| Loops | Loops | Int32 | (Inherited from Abstract animation) |