Duration
Display Duration data
- BrowseName
- DurationPicker
- SuperType
- Element(Item)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Value | Value | Duration | Value displayed and possibly changed by the user |
| Font family | FontFamily | Font | Font family |
| Font weight | FontWeight | Font weight | Font weight |
| Font italic | FontItalic | Boolean | Enables/disables italics in the text |
| Font size | FontSize | Size | Font size |
| Text color | TextColor | Color | Color of the text to display |
| Control in read-only mode | ReadOnly | Boolean | Enables/disables the read-only mode. If enabled, it is not possible to write in the text box but. For example, it is possible to select the existing text for copy-paste |
| Text horizontal alignment | TextHorizontalAlignment | Text horizontal alignment | Indicates where the text is positioned on the horizontal axis |
| Text vertical alignment | TextVerticalAlignment | Text vertical alignment | Indicates where the text is positioned on the vertical axis |
| Border color | BorderColor | Color | Color of the polygon border |
| Style | Style | String | Graphic style applied to the control |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |
Events
Modified value
- BrowseName
- Modified value
Event that is triggered when the user changes the value of the control