Label style
Styles for labels
- BrowseName
- LabelStyle
- SuperType
- Control style(ControlStyle)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Text color | TextColor | Color | Color of the text to display |
| Font family | FontFamily | Font | Font family |
| Font weight | FontWeight | Font weight | Font weight |
| Font italic | FontItalic | Boolean | Enables/disables italics in the text |
| Font underline | FontUnderline | Boolean | Enables/disables underline in the text |
| Font size | FontSize | Size | Font size |
| Background color | BackgroundColor | Color | If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property |
| Radius | Radius | Size | Radius of the angles of the objects |