PolyLine
PolyLine that can be adapted to fit the design needs
- BrowseName
- PolyLine
- SuperType
- Container(Container)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Border color | LineColor | Color | Color of the polygon border |
| Fill color | FillColor | Color | Fill color of the polygon area |
| Thickness | LineThickness | Size | Line thickness |
| Blink | Blink | Boolean | Allows the object to periodically blink, ignored when the object is not visible |
| Path | Path | String | Path |
| Hit test visible | HitTestVisible | Boolean | True: intercept user clicks. False: does not intercept user clicks, which are instead passed to the underlying object, based on the order on the Z axis |
| Move target | MoveTarget | NodeId | (Inherited from Container) |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |
Events
MouseDown event
- BrowseName
- MouseDown event
Event that is triggered when the left mouse button is pressed (falling edge)
MouseUp event
- BrowseName
- MouseUp event
Event that is triggered when the left mouse button is released (rising edge)