Presentation engine
Create interactive sessions at runtime
- BrowseName
- PresentationEngine
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Start window | StartWindow | NodeId | Type of start Window object to create at the start of the session |
| LoginWindow | LoginWindow | NodeId | Type of login Window object that is prompted at the start of the session when you are not logged in |
| Style sheet | StyleSheet | NodeId | Set the styles of graphical objects, either globally or for specific object classes |
| Starting user | StartingUser | NodeId | The starting user with which to authenticate the session |
| Session | Session | NodeId | UISession object to use |
| Sessions | UI Session |