Label
Visualizes a text
- BrowseName
- Label
- SuperType
- Element(Item)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Text | Text | LocalizedText | Text inserted and displayed |
| Text horizontal alignment | TextHorizontalAlignment | Text horizontal alignment | Indicates where the text is positioned on the horizontal axis |
| Text vertical alignment | TextVerticalAlignment | Text vertical alignment | Indicates where the text is positioned on the vertical axis |
| Word wrap | WordWrap | Boolean | Enable/disable the automatic word wrapping when the text is wider than the container. Ignored when the object width is automatic or when text abbreviation is set |
| Text trimming | Elide | Text trimming | Text trimming mode. Insert three dots (...) in the indicated position when the text is too long for the available space. Ignored when the object width is automatic or when word wrap is set |
| Font family | FontFamily | Font | Font family |
| Font weight | FontWeight | Font weight | Font weight |
| Font italic | FontItalic | Boolean | Enables/disables italics in the text |
| Font underline | FontUnderline | Boolean | Enables/disables underline in the text |
| Font size | FontSize | Size | Font size |
| Text color | TextColor | Color | Color of the text to display |
| Blink | Blink | Boolean | Allows the object to periodically blink, ignored when the object is not visible |
| Style | Style | String | Graphic style applied to the control |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |