Array line pen
XY chart object pen that draws a line whose points represent both dimensions of a two-dimensional matrix variable
- BrowseName
- XYChartArrayLinePen
- SuperType
- XY chart line(XYChartLinePen)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Point array | PointArray | Number | Bidimensional array of X, X coordinates that should be drawn by the chart |
| Editable | Editable | Boolean | Enable/disable the change of the value directly in the chart |
| Color | Color | Color | (Inherited from XY chart line) |
| Thickness | Thickness | Size | (Inherited from XY chart line) |
| Enabled | Enabled | Boolean | (Inherited from XY chart pen) |