DateTimeAxis
Time X axis of a Trend Graph
- BrowseName
- DateTimeAxis
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Follow | Follow | Boolean | Enable/disable automatic scrolling on the X axis |
| Time window | Window | Duration | Time interval in hours displayed on the X axis |
| Interactive | Interactive | Boolean | Enable/disable interactivity with the axes |
| Date and time | Time | DateTime | Start date and time on the X axis. Is set in UTC and displayed in local time. Is the current time by default |
| Snap position | SnapPosition | Snap position |