InfluxDB database
Object that represents an InfluxDB
- BrowseName
- InfluxDBStore
- SuperType
- Store(Store)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Token | Token | Password | Database access token |
| Organization | Organization | String | Name of the organiazation in the database server |
| Bucket | Bucket | String | Name of the bucket in the database server |
| Server | Server | String | IP address or hostname of the database server in the network |
| TCP Port | Port | UInt16 | TCP port of the database server |
| Use SSL | UseSSL | Boolean | Use SSL |
| Server Certificate | ServerCertificate | ResourceUri | Server certificate |
| Tables | Tables | InfluxDB store table | (Inherited from Store) |
| Max column name length | MaxColumnNameLength | UInt32 | (Inherited from Store) |
| Max columns count | MaxColumnCount | UInt32 | (Inherited from Store) |
| Data type compatibility map | DataTypeCompatibilityMap | NodeId | (Inherited from Store) |
| Status | Status | Store status | (Inherited from Store) |