Deploying projects
Compile projects to FactoryTalk Optix Applications and then deploy the applications to target devices.
To determine which presentation engine is required for the mode in which FactoryTalk Optix will be running, see FactoryTalk Optix runtime modes.
You can manage the target devices to which you deploy FactoryTalk Optix Applications. See Manage client devices and Deploy a FactoryTalk Optix Application.
For target devices not accessible in the network, you can export FactoryTalk Optix Applications from FactoryTalk Optix Studio and then import them to target devices. See Export a FactoryTalk Optix Application and Import a FactoryTalk Optix Application.