Value axis
Y axis of the values of a Trend Graph
- BrowseName
- ValueAxis
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Minimum value | MinValue | Size | Minimum value displayed on the Y axis |
| Maximum value | MaxValue | Size | Maximum value displayed on the Y axis |
| Automatic scaling | AutoScale | Boolean | Enable/disable resizing of the Y axis based on the minimum and maximum values displayed in the graphic at runtime |
| Interactive | Interactive | Boolean | Enable/disable interactivity with the axes |
| Position | Position | Horizontal position | Position of the scale relative to the control |