Container
Container of FTOptix elements
- BrowseName
- Container
- SuperType
- Element(Item)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Move target | MoveTarget | NodeId | Reference to the container that will be moved when a move action is performed on the current container |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |