Vertical layout
Panel that automatically arranges the directly child graphical objects vertically next to each other
- BrowseName
- ColumnLayout
- SuperType
- Container(Container)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Content alignment | ContentAlignment | Content vertical alignment | Horizontal alignment of children. Left aligned: children are anchored to the left side, Center aligned: children are anchored to the center; Right aligned: children are anchored to the right side |
| Wrap | Wrap | Boolean | Set the wrap mode for the layout's content |
| Horizontal gap | HorizontalGap | Size | Space between columns in the layout |
| Vertical gap | VerticalGap | Size | Space between rows of the layout |
| Move target | MoveTarget | NodeId | (Inherited from Container) |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |