Scale layout
Panel that automatically scales the child graphical objects
- BrowseName
- ScaleLayout
- SuperType
- Container(Container)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Fill Mode | FillMode | Fill mode | Fill mode of the image object (Fit: resize the image keeping the original aspect ratio, Stretch: resize the image by fitting the aspect ratio to the area of the image object) |
| Original width | OriginalWidth | Size | The original width of the scale layout |
| Original height | OriginalHeight | Size | The original height of the scale layout |
| Font scaling | FontScaling | Boolean | |
| Move target | MoveTarget | NodeId | (Inherited from Container) |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |