Event configuration
Configuration of an event type to monitor through Events logger
- BrowseName
- EventConfiguration
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Event source | EventSource | NodeId | Source node of the events of interest. If empty, considers the events of interest generated by any project object |
| Listen subtree | MonitorSubtree | Boolean | If True, sources child nodes of the node selected in Event source |
| Event type | EventType | NodeId | Type of event for which to record the data |
| Non-interactive sessions excluded | ExcludeNonInteractiveSessions | Boolean | Records only the events generated by user interactions with the application graphical interface and ignores events generated by other logics |