Spin box
Increase/decrease a numerical value using buttons or keyboard
- BrowseName
- SpinBox
- SuperType
- Element(Item)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Value | Value | Double | Value displayed and possibly changed by the user |
| Minimum value | MinValue | Double | Minimum value displayed on the Y axis |
| Maximum value | MaxValue | Double | Maximum value displayed on the Y axis |
| Increment | Increment | Double | Added or subtracted value (for example, 1, 0.1, or 0.01) using buttons |
| Input format | Format | String | Format of the value that is presented to the user (such as decimal digits, leading zeroes, etc) |
| Editable | Editable | Boolean | Enable/disable the change of the value directly in the chart |
| Show buttons | ShowButtons | Boolean | Show buttons to increase or decrease current value |
| Font family | FontFamily | Font | Font family |
| Font weight | FontWeight | Font weight | Font weight |
| Font italic | FontItalic | Boolean | Enables/disables italics in the text |
| Font size | FontSize | Size | Font size |
| Text color | TextColor | Color | Color of the text to display |
| Input box style | InputBoxStyle | String | Style for input controls |
| Button style | ButtonStyle | String | Style for buttons |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |
Events
Modified value
- BrowseName
- Modified value
Event that is triggered when the user changes the value of the control