Data grid column
Data grid object column
- BrowseName
- DataGridColumn
- SuperType
- Object(BaseObjectType)
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Title | Title | LocalizedText | Panel title, to be displayed in the navigation tab of a Navigation panel object. If not set, the panel BrowseName is displayed |
Width | Width | Size | Width of column. Auto resizes columns when the Data grid is resized. Numeric value maintains specified column size when the Data grid is resized |
Visible | Visible | Boolean | Show/hide the window |
Header alignment | HeaderAlignment | Text horizontal alignment | Horizontal alignment of the content in the header row |
Content alignment | ContentAlignment | Horizontal alignment | Horizontal alignment of the content in the rows other than the header row |
Order by | OrderBy | NodePath | Attribute/property of the nodes or column of a table by which to sort the elements. Generally the same attribute/property or column from which the elements are obtained is set |
Data item template | DataItemTemplate | Data grid template element | Data item template object which can contain data in textual or image format |