MouseClick event
Event that is triggered when the left mouse button is pressed and then released
- BrowseName
- MouseClickEvent
- SuperType
- Mouse event(MouseEvent)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| EventId | ByteString | (Inherited from BaseEventType) | |
| EventType | NodeId | (Inherited from BaseEventType) | |
| SourceNode | NodeId | (Inherited from BaseEventType) | |
| SourceName | String | (Inherited from BaseEventType) | |
| Time | UtcTime | (Inherited from BaseEventType) | |
| ReceiveTime | UtcTime | (Inherited from BaseEventType) | |
| LocalTime | TimeZoneDataType | (Inherited from BaseEventType) | |
| Message | LocalizedText | (Inherited from BaseEventType) | |
| Severity | UInt16 | (Inherited from BaseEventType) | |
| ConditionClassId | NodeId | (Inherited from BaseEventType) | |
| ConditionClassName | LocalizedText | (Inherited from BaseEventType) | |
| ConditionSubClassId | NodeId | (Inherited from BaseEventType) | |
| ConditionSubClassName | LocalizedText | (Inherited from BaseEventType) |