XY chart
Displays the value of two-dimensional variables in a Cartesian chart
- BrowseName
- XYChart
- SuperType
- Element(Item)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Zoom | Zoom | Double | Zoom level of the chart. <1: zoom backward; >1: zoom forward |
| Center X | CenterX | Double | X coordinate in relation to which to center the chart |
| Center Y | CenterY | Double | Y coordinate in relation to which to center the chart |
| Key visible | LegendVisible | Boolean | Show/hide the legend of the pens |
| Style | Style | String | Graphic style applied to the control |
| Pens | Pens | XY chart pen | Trend lines. Trend pen collection of objects |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |
Methods
Refresh
- BrowseName
- Refresh
Refresh the displayed data