Embedded database
Object that represents an SQLite project embedded database at runtime
- BrowseName
- SQLiteStore
- SuperType
- Store(Store)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| In memory | InMemory | Boolean | Enable/disable non-persistent storage mode. In this mode, the store content is no longer available when the FactoryTalk Optix Application is restarted |
| Filename | Filename | String | Customized name of the database file |
| Tables | Tables | SQLite store table | (Inherited from Store) |
| Max column name length | MaxColumnNameLength | UInt32 | (Inherited from Store) |
| Max columns count | MaxColumnCount | UInt32 | (Inherited from Store) |
| Data type compatibility map | DataTypeCompatibilityMap | NodeId | (Inherited from Store) |
| Status | Status | Store status | (Inherited from Store) |
Methods
Backup
- BrowseName
- Backup
Performs a hot backup to file of the embedded database
| Name | DataType | Description |
|---|---|---|
| OutputFilePath | ResourceUri | Path to the backup file |
| Name | DataType | Description |
|---|---|---|
| Result | Boolean | Result of the backup operation |
Restore
- BrowseName
- Restore
Performs a hot restore from file of the embedded database
| Name | DataType | Description |
|---|---|---|
| InputFilePath | ResourceUri | Path to the file to be restored |
| Name | DataType | Description |
|---|---|---|
| Result | Boolean | Result of the restore operation |