Tooltip style
Style for tooltips
- BrowseName
- ToolTipStyle
- SuperType
- Control style(ControlStyle)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Background color | BackgroundColor | Color | If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property |
| Text color | TextColor | Color | Color of the text to display |
| Border color | BorderColor | Color | Color of the polygon border |
| Border width | BorderWidth | Size | Thickness of the object border |
| Font family | FontFamily | Font | Font family |
| Font weight | FontWeight | Font weight | Font weight |
| Font italic | FontItalic | Boolean | Enables/disables italics in the text |
| Font size | FontSize | Size | Font size |
| Radius | Radius | Size | Radius of the angles of the objects |