Direct Drives Connectivity
Use Direct Drive Connectivity feature in your projects to enable PowerFlex drives.
The Direct Drive Connectivity allows to:
- Create information model of PowerFlex, basing on drive predefined profiles
- Create client and read data from PowerFlex drives. Four types of PowerFlex drives are supported: PF755, PF755TM, PF6000T, and PF7000
Tip:
The Direct Drive Connectivity is supported only on Windows® operating systems.