Popup
A window that appears in response to a user interaction. Can be used for error handling, confirmation messages, status notifications, or other just-in-time user information
- BrowseName
- Popup
- SuperType
- Container(Container)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Move target | MoveTarget | NodeId | (Inherited from Container) |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |
Methods
Close
- BrowseName
- Close
Close the current object or selection