System object
The System object provides the network configuration for your system through network and IP settings. Add the System object to access system settings such as date and time and IP addresses of the network interfaces at runtime or to restart the system.
Adding the System object to your project automatically displays DateAndTime, Device, Display, and Application property categories. Bind these properties to variables using the Dynamic Link browser.
At runtime, the network interface properties are automatically added to the System object properties and display the current settings. For example, if the system has a LAN network interface that is configured with two additional IP addresses, at runtime, the System object properties contain a Network interfaces category with additional IP addresses for the LAN network.