Multistate image
Based on the current state value, displays a specific image
- BrowseName
- MultiStateImage
- SuperType
- Image(Image)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| State value | StateValue | Int32 | Value of the current state |
| States | States | MultiStateImageState | List of states, each of which is associated with a specific image |
| Path | Path | ResourceUri | (Inherited from Image) |
| Dynamic color | DynamicColor | Color | (Inherited from Image) |
| Fill Mode | FillMode | Fill mode | (Inherited from Image) |
| Hit test visible | HitTestVisible | Boolean | (Inherited from Image) |
| Image left margin | ImageLeftMargin | Size | (Inherited from Image) |
| Image top margin | ImageTopMargin | Size | (Inherited from Image) |
| Image right margin | ImageRightMargin | Size | (Inherited from Image) |
| Image bottom margin | ImageBottomMargin | Size | (Inherited from Image) |
| Blink | Blink | Boolean | (Inherited from Image) |
| Colorization mode | ColorizationMode | Colorization mode | (Inherited from Image) |
| Move target | MoveTarget | NodeId | (Inherited from Container) |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |