Navigation panel style
Style for navigation panels
- BrowseName
- NavigationPanelStyle
- SuperType
- Control style(ControlStyle)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Color | InactiveColor | Color | Color of the range |
| Inactive text color | InactiveTextColor | Color | Text color of an inactive element |
| Active primary color | ActivePrimaryColor | Color | Color used to indicate the currently selected tab's color |
| Active secondary color | ActiveSecondaryColor | Color | Color used to indicate the text color of the currently selected tab, ignored when Appearance: Underlined |
| Background color | BackgroundColor | Color | If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property |
| Font family | FontFamily | Font | Font family |
| Font weight | FontWeight | Font weight | Font weight |
| Font italic | FontItalic | Boolean | Enables/disables italics in the text |
| Font size | FontSize | Size | Font size |
| Radius | Radius | Size | Radius of the angles of the objects |
| Icon uses text color | IconUsesTextColor | Boolean | When True the tab's icon will be colorized like the tab's text |
| Tab spacing | TabSpacing | Size | Set the space between tabs |
| Tab padding | TabPadding | Size | Padding between the Navigation Panel tab buttons and the bar |