Button style
Style for buttons
- BrowseName
- ButtonStyle
- SuperType
- Control style(ControlStyle)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Color | Color | Color | Color of the pen line |
| Border color | BorderColor | Color | Color of the polygon border |
| Text color | TextColor | Color | Color of the text to display |
| Pressed color | PressedColor | Color | Color of the element while is being pressed |
| Pressed border color | PressedBorderColor | Color | Border color of the element while is being pressed |
| Pressed text color | PressedTextColor | Color | Text color of the element while is being pressed |
| Focus border color | FocusBorderColor | Color | Border color of the element while is being selected |
| Font family | FontFamily | Font | Font family |
| Font weight | FontWeight | Font weight | Font weight |
| Font italic | FontItalic | Boolean | Enables/disables italics in the text |
| Font size | FontSize | Size | Font size |
| Border width | BorderWidth | Size | Thickness of the object border |
| Radius | Radius | Size | Radius of the angles of the objects |
| Icon uses text color | IconUsesTextColor | Boolean | When True the tab's icon will be colorized like the tab's text |
| Horizontal padding percent | HorizontalPaddingPercent | Float | Percentage of the distance between the content and the horizontal edges of the objects |
| Vertical padding percent | VerticalPaddingPercent | Float | Percentage of the distance between the content and the vertical edges of the objects |