Retentivity storage
Store on which the runtime changes are saved
- BrowseName
- RetentivityStorage
- SuperType
- NodeLoader(NodeLoader)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Write delay | WriteDelay | Duration | Defines how often to save changes. The default value is zero, when a change is detected, it is saved in real time |
| Delta observer enabled | DeltaObserverEnabled | Boolean | Disables new additions to the retentivity storage, only data that is already saved are loaded when the application starts, no new data is added |
| Nodes | Nodes | Node pointer |