Element
Generic FTOptix element
- BrowseName
- Item
- SuperType
- Base UI object type(BaseUIObject)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Visible | Visible | Boolean | Show/hide the window |
| Enabled | Enabled | Boolean | Enables/disables the interaction with the user (True: enabled; False: disabled) |
| Opacity | Opacity | Float | Opacity level (0: transparent) |
| Left margin | LeftMargin | Size | (Only if Horizontal Alignment: Left or Center or Stretch) Distance between the left edge of the object and the left edge of its container |
| Top margin | TopMargin | Size | (Only if Vertical Alignment: Top or Center or Stretch) Distance between the top edge of the object and the top edge of its container |
| Right margin | RightMargin | Size | (Only if Horizontal Alignment: Right or Center or Stretch) Distance between the right edge of the object and the right edge of its container |
| Bottom margin | BottomMargin | Size | (Only if Vertical Alignment: Bottom or Center or Stretch) Distance between the bottom edge of the object and the bottom edge of its container |
| Width | Width | Size | Width of the window. It can assume values greater than or equal to zero. The Auto value sets the width equal to the width of the content (in this case, in the absence of content the object collapses) |
| Height | Height | Size | Height of the window. It can assume values greater than or equal to zero. The Auto value sets the height equal to the height of the content (in this case, in the absence of content the object collapses) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | Alignment of the object on the horizontal axis. Left: the left side is positioned on the left side of the container, except for the left margin; Right: the right side is positioned on the right side of the container, except for the right margin; Center: the center of the object is positioned in the center of the container, except for the left and/or right margins; Stretch: object width equals container width, except for the left and/or right margins |
| Vertical alignment | VerticalAlignment | Vertical alignment | Alignment of the object on the vertical axis. Top: the top side is positioned on the top side of the container, except for the top margin; Bottom: the bottom side is positioned on the bottom side of the container, except for the bottom margin; Center: the center of the object is positioned in the center of the container, except for the top and/or bottom margins; Stretch: object height equals container height, except for the top and/or bottom margins |
| Rotation | Rotation | Size | Rotation of the object around its center point. Positive values indicate clockwise arc degrees |