PDF generation result
Result code of the PDF generation
- BrowseName
- GeneratePdfCompletedResult
Values
| Value | DisplayName | Description |
|---|---|---|
| 0 | PDF generated successfully | PDF has been generated |
| 1 | Unsupported locale | The specified locale is not available |
| 2 | Failed to process report template | Cannot process the input template |
| 3 | Unable to overwrite output file | The output file cannot be overwritten |
| 4 | Unable to generate PDF | PDF cannot be generated |
| 5 | Empty or invalid output resource URI | The specified output path is not valid |