Graphic objects
Use predefined graphic objects to add visual components to FactoryTalk Optix Applications. Use Presentation Engines to display the UI at runtime on different viewports.
FactoryTalk Optix Studio includes predefined graphic objects to add and arrange in the visual editor. See Predefined graphic objects and Editor.
In Project view and in the editor, create, duplicate, edit, and set the properties of graphic object instances and graphic object types. See Manage graphic objects and Graphic objects layout.