Gauge style
Style for gauges
- BrowseName
- GaugeStyle
- SuperType
- Control style(ControlStyle)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Background color | BackgroundColor | Color | If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property |
| Foreground color | ForegroundColor | Color | Color of the element that is on the higher Z order |
| Border color | BorderColor | Color | Color of the polygon border |
| Border width | BorderWidth | Size | Thickness of the object border |
| Text color | TextColor | Color | Color of the text to display |
| Font family | FontFamily | Font | Font family |
| Font weight | FontWeight | Font weight | Font weight |
| Font italic | FontItalic | Boolean | Enables/disables italics in the text |
| Font size | FontSize | Size | Font size |
| Handle color | HandleColor | Color | Color of the element's handle |
| Handle border color | HandleBorderColor | Color | Color of the handle border |
| Handle border width | HandleBorderWidth | Size | Width of the handle border |
| Handle size | HandleSize | Size | Size of the handle |
| Radius | Radius | Size | Radius of the angles of the objects |
| Tooltip background color | ToolTipBackgroundColor | Color | Background color of the tooltip |
| Tooltip text color | ToolTipTextColor | Color | Text color of the tooltip |