Libraries
Libraries contain object definitions that you can add to your projects.
Library types
| Type | Description |
|---|---|
|
Template library |
The default library of objects that you cannot edit or remove. Template libraries are provided for:
|
|
Custom library |
A library created by a user that contains a set of objects either curated from the template libraries or customized for specific automation scenarios. |
Library repositories
You can store libraries locally or in a remote Git repository. Libraries are available across FactoryTalk Optix projects.
Libraries are saved in the C:\Users\UserName\Documents\Rockwell Automation\FactoryTalk Optix\Libraries folder.
Library updates
Libraries and library objects are tied to the version of the FactoryTalk Optix software with which they were originally configured. When you install an updated version, FactoryTalk Optix updates the built-in template libraries to make the libraries compatible with the new software.
If your project contains custom libraries that use components that changed in the updated version of FactoryTalk Optix, you must manually update the custom libraries.