Navigation panel
Panel that contains other panels and automatically organizes them into navigable tabs
- BrowseName
- NavigationPanel
- SuperType
- Container(Container)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Attached panel loader | AttachedPanelLoader | NodeId | The Panel Loader to be used to show the navigation panel's content |
| Current panel | CurrentPanel | NodeId | Node ID of the node of the panel displayed |
| Tab position | TabPosition | Tab position | Position of the navigation tabs on the y axis |
| Tab height | TabHeight | Size | Sets the height for all the tabs. When Auto the height of all tabs adjusts to that of the highest tab |
| Tab width | TabWidth | Size | Set the width for all the tabs, when set all tabs have a fixed size. When Auto tabs automatically adjust their width to their content's width |
| Current tab index | CurrentTabIndex | Int32 | Index of the currently selected tab |
| Appearance | Appearance | String | NavigationPanel's appearance |
| Style | Style | String | Graphic style applied to the control |
| Panels | Panels | Navigation panel item | Collection of Panel objects to display |
| Move target | MoveTarget | NodeId | (Inherited from Container) |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |
Methods
Change panel by tab index
- BrowseName
- ChangePanelByTabIndex
Changes the current panel by providing the index of the desired tab