Text box
Insert and view a text at runtime
- BrowseName
- TextBox
- SuperType
- Element(Item)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Text | Text | LocalizedText | Text inserted and displayed |
| Text horizontal alignment | TextHorizontalAlignment | Text horizontal alignment | Indicates where the text is positioned on the horizontal axis |
| Text vertical alignment | TextVerticalAlignment | Text vertical alignment | Indicates where the text is positioned on the vertical axis |
| Value change behavior | ValueChangeBehaviour | Value change behavior | Mode of updating text when the user writes in the text box. At end of typing: update the value after the user has pressed Enter with either physical or virtual keyboard (pressing Esc or clicking outside the object, the previous text is restored); When typing: in real-time when writing |
| Font family | FontFamily | Font | Font family |
| Font weight | FontWeight | Font weight | Font weight |
| Font italic | FontItalic | Boolean | Enables/disables italics in the text |
| Font size | FontSize | Size | Font size |
| Text color | TextColor | Color | Color of the text to display |
| Border color | BorderColor | Color | Color of the polygon border |
| Placeholder text | PlaceholderText | LocalizedText | Text to display when the box is empty, typically an example or indication for the user |
| Control in read-only mode | ReadOnly | Boolean | Enables/disables the read-only mode. If enabled, it is not possible to write in the text box but. For example, it is possible to select the existing text for copy-paste |
| Content Type | ContentType | Input type | Content type. Normal: characters displayed; Password: characters hidden |
| Style | Style | String | Graphic style applied to the control |
| Visible | Visible | Boolean | (Inherited from Element) |
| Enabled | Enabled | Boolean | (Inherited from Element) |
| Opacity | Opacity | Float | (Inherited from Element) |
| Left margin | LeftMargin | Size | (Inherited from Element) |
| Top margin | TopMargin | Size | (Inherited from Element) |
| Right margin | RightMargin | Size | (Inherited from Element) |
| Bottom margin | BottomMargin | Size | (Inherited from Element) |
| Width | Width | Size | (Inherited from Element) |
| Height | Height | Size | (Inherited from Element) |
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | (Inherited from Element) |
| Vertical alignment | VerticalAlignment | Vertical alignment | (Inherited from Element) |
| Rotation | Rotation | Size | (Inherited from Element) |