Dialog box
Window that can be made modal, i.e. not allowing interaction with other interface elements
- BrowseName
 - Dialog
 - SuperType
 - Container(Container)
 
Properties
| Name | BrowseName | DataType | Description | 
|---|---|---|---|
| Modal dialog window | Modal | Boolean | Enable/disable the behavior as modal window | 
| Horizontal alignment | HorizontalAlignment | Horizontal alignment | Alignment of the object on the horizontal axis. Left: the left side is positioned on the left side of the container, except for the left margin; Right: the right side is positioned on the right side of the container, except for the right margin; Center: the center of the object is positioned in the center of the container, except for the left and/or right margins; Stretch: object width equals container width, except for the left and/or right margins | 
| Vertical alignment | VerticalAlignment | Vertical alignment | Alignment of the object on the vertical axis. Top: the top side is positioned on the top side of the container, except for the top margin; Bottom: the bottom side is positioned on the bottom side of the container, except for the bottom margin; Center: the center of the object is positioned in the center of the container, except for the top and/or bottom margins; Stretch: object height equals container height, except for the top and/or bottom margins | 
| Move target | MoveTarget | NodeId | (Inherited from Container) | 
| Visible | Visible | Boolean | (Inherited from Element) | 
| Enabled | Enabled | Boolean | (Inherited from Element) | 
| Opacity | Opacity | Float | (Inherited from Element) | 
| Left margin | LeftMargin | Size | (Inherited from Element) | 
| Top margin | TopMargin | Size | (Inherited from Element) | 
| Right margin | RightMargin | Size | (Inherited from Element) | 
| Bottom margin | BottomMargin | Size | (Inherited from Element) | 
| Width | Width | Size | (Inherited from Element) | 
| Height | Height | Size | (Inherited from Element) | 
| Rotation | Rotation | Size | (Inherited from Element) | 
Methods
Close
- BrowseName
 - Close
 
Close the current object or selection