ScrollBar style
Style for scrollbars
- BrowseName
- ScrollBarStyle
- SuperType
- Control style(ControlStyle)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| ScrollBar auto hide | AutoHide | Boolean | Auto hide scroll bars if not needed |
| Background color | BackgroundColor | Color | If the Appearance is Default, Bordered Circular or Bordered Rectangular, it is the color of the button. If the Appearance is Accent, the color is the one set in the style sheet in the Highlight color property |
| Size | Size | Size | Size of the element |
| Handle color | HandleColor | Color | Color of the element's handle |
| Handle border color | HandleBorderColor | Color | Color of the handle border |
| Handle border width | HandleBorderWidth | Size | Width of the handle border |
| Handle radius | HandleRadius | Size | Radius of the handle |
| Radius | Radius | Size | Radius of the angles of the objects |
| Show buttons | ShowButtons | Boolean | Show buttons to increase or decrease current value |