Grid Layout Properties
Properties for graphic object placement in a grid layout
- BrowseName
- GridLayoutProperties
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Column Start | ColumnStart | Int32 | Column in which to start a grid item |
| Column Span | ColumnSpan | Int32 | Number of columns that the item should take in Grid Layout |
| Row Start | RowStart | Int32 | Row in which to start a grid item |
| Row Span | RowSpan | Int32 | Number of rows in the grid layout taken up by an item |