Tab position
Position of the tabs for the control
- BrowseName
- NavigationPanelTabPositionEnum
Values
| Value | DisplayName | Description |
|---|---|---|
| 0 | Top | Tabs are displayed above the control |
| 1 | Bottom | Tabs are displayed below of the control |
| 2 | Left | Tabs are displayed on the left of the control |
| 3 | Right | Tabs are displayed on the right of the control |
| 4 | Hidden | No tabs are displayed |