WriterGroupType
- BrowseName
- WriterGroupType
- SuperType
- PubSubGroupType(PubSubGroupType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| WriterGroupId | UInt16 | ||
| PublishingInterval | Duration | ||
| KeepAliveTime | Duration | ||
| Priority | Byte | ||
| LocaleIds | LocaleId | ||
| HeaderLayoutUri | String | ||
| TransportSettings | WriterGroupTransportType | ||
| MessageSettings | WriterGroupMessageType | ||
| <DataSetWriterName> | |||
| Diagnostics | |||
| SecurityMode | MessageSecurityMode | (Inherited from PubSubGroupType) | |
| SecurityGroupId | String | (Inherited from PubSubGroupType) | |
| SecurityKeyServices | EndpointDescription | (Inherited from PubSubGroupType) | |
| MaxNetworkMessageSize | UInt32 | (Inherited from PubSubGroupType) | |
| GroupProperties | KeyValuePair | (Inherited from PubSubGroupType) | |
| Status | (Inherited from PubSubGroupType) |
Methods
AddDataSetWriter
- BrowseName
- AddDataSetWriter
| Name | DataType | Description |
|---|---|---|
| Configuration | DataSetWriterDataType |
| Name | DataType | Description |
|---|---|---|
| DataSetWriterNodeId | NodeId |
RemoveDataSetWriter
- BrowseName
- RemoveDataSetWriter
| Name | DataType | Description |
|---|---|---|
| DataSetWriterNodeId | NodeId |