PubSubConfigurationType
- BrowseName
- PubSubConfigurationType
- SuperType
- FileType(FileType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| Size | UInt64 | (Inherited from FileType) | |
| Writable | Boolean | (Inherited from FileType) | |
| UserWritable | Boolean | (Inherited from FileType) | |
| OpenCount | UInt16 | (Inherited from FileType) | |
| MimeType | String | (Inherited from FileType) | |
| MaxByteStringLength | UInt32 | (Inherited from FileType) | |
| LastModifiedTime | DateTime | (Inherited from FileType) |
Methods
ReserveIds
- BrowseName
- ReserveIds
| Name | DataType | Description |
|---|---|---|
| TransportProfileUri | String | |
| NumReqWriterGroupIds | UInt16 | |
| NumReqDataSetWriterIds | UInt16 |
| Name | DataType | Description |
|---|---|---|
| DefaultPublisherId | BaseDataType | |
| WriterGroupIds | UInt16 | |
| DataSetWriterIds | UInt16 |
CloseAndUpdate
- BrowseName
- CloseAndUpdate
| Name | DataType | Description |
|---|---|---|
| FileHandle | UInt32 | |
| RequireCompleteUpdate | Boolean | |
| ConfigurationReferences | PubSubConfigurationRefDataType |
| Name | DataType | Description |
|---|---|---|
| ChangesApplied | Boolean | |
| ReferencesResults | StatusCode | |
| ConfigurationValues | PubSubConfigurationValueDataType | |
| ConfigurationObjects | NodeId |