DataSetReaderType
- BrowseName
- DataSetReaderType
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| PublisherId | BaseDataType | ||
| WriterGroupId | UInt16 | ||
| DataSetWriterId | UInt16 | ||
| DataSetMetaData | DataSetMetaDataType | ||
| DataSetFieldContentMask | DataSetFieldContentMask | ||
| MessageReceiveTimeout | Duration | ||
| KeyFrameCount | UInt32 | ||
| HeaderLayoutUri | String | ||
| SecurityMode | MessageSecurityMode | ||
| SecurityGroupId | String | ||
| SecurityKeyServices | EndpointDescription | ||
| DataSetReaderProperties | KeyValuePair | ||
| TransportSettings | DataSetReaderTransportType | ||
| MessageSettings | DataSetReaderMessageType | ||
| Status | |||
| Diagnostics | |||
| SubscribedDataSet | SubscribedDataSetType |
Methods
CreateTargetVariables
- BrowseName
- CreateTargetVariables
| Name | DataType | Description |
|---|---|---|
| ConfigurationVersion | ConfigurationVersionDataType | |
| TargetVariablesToAdd | FieldTargetDataType |
| Name | DataType | Description |
|---|---|---|
| AddResults | StatusCode |
CreateDataSetMirror
- BrowseName
- CreateDataSetMirror
| Name | DataType | Description |
|---|---|---|
| ParentNodeName | String | |
| RolePermissions | RolePermissionType |
| Name | DataType | Description |
|---|---|---|
| ParentNodeId | NodeId |