ApplicationConfigurationType
- BrowseName
- ApplicationConfigurationType
- SuperType
- ServerConfigurationType(ServerConfigurationType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| ApplicationUri | UriString | ||
| ProductUri | UriString | ||
| ApplicationType | ApplicationType | ||
| Enabled | Boolean | ||
| ServerCapabilities | String | (Inherited from ServerConfigurationType) | |
| SupportedPrivateKeyFormats | String | (Inherited from ServerConfigurationType) | |
| MaxTrustListSize | UInt32 | (Inherited from ServerConfigurationType) | |
| MulticastDnsEnabled | Boolean | (Inherited from ServerConfigurationType) | |
| HasSecureElement | Boolean | (Inherited from ServerConfigurationType) | |
| CertificateGroups | (Inherited from ServerConfigurationType) | ||
| TransactionDiagnostics | (Inherited from ServerConfigurationType) |