ConditionType
- BrowseName
- ConditionType
- SuperType
- BaseEventType(BaseEventType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| ConditionClassId | NodeId | ||
| ConditionClassName | LocalizedText | ||
| ConditionName | String | ||
| BranchId | NodeId | ||
| Retain | Boolean | ||
| SupportsFilteredRetain | Boolean | ||
| EnabledState | LocalizedText | ||
| Quality | StatusCode | ||
| LastSeverity | UInt16 | ||
| Comment | LocalizedText | ||
| ClientUserId | String | ||
| EventId | ByteString | (Inherited from BaseEventType) | |
| EventType | NodeId | (Inherited from BaseEventType) | |
| SourceNode | NodeId | (Inherited from BaseEventType) | |
| SourceName | String | (Inherited from BaseEventType) | |
| Time | UtcTime | (Inherited from BaseEventType) | |
| ReceiveTime | UtcTime | (Inherited from BaseEventType) | |
| LocalTime | TimeZoneDataType | (Inherited from BaseEventType) | |
| Message | LocalizedText | (Inherited from BaseEventType) | |
| Severity | UInt16 | (Inherited from BaseEventType) | |
| ConditionSubClassId | NodeId | (Inherited from BaseEventType) | |
| ConditionSubClassName | LocalizedText | (Inherited from BaseEventType) |
Methods
Disable
- BrowseName
- Disable
Enable
- BrowseName
- Enable
Add Comment
- BrowseName
- AddComment
| Name | DataType | Description |
|---|---|---|
| EventId | ByteString | |
| Comment | LocalizedText |
Condition Refresh
- BrowseName
- ConditionRefresh
| Name | DataType | Description |
|---|---|---|
| SubscriptionId | IntegerId |