ReaderGroupType
- BrowseName
- ReaderGroupType
- SuperType
- PubSubGroupType(PubSubGroupType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| <DataSetReaderName> | |||
| Diagnostics | |||
| TransportSettings | ReaderGroupTransportType | ||
| MessageSettings | ReaderGroupMessageType | ||
| SecurityMode | MessageSecurityMode | (Inherited from PubSubGroupType) | |
| SecurityGroupId | String | (Inherited from PubSubGroupType) | |
| SecurityKeyServices | EndpointDescription | (Inherited from PubSubGroupType) | |
| MaxNetworkMessageSize | UInt32 | (Inherited from PubSubGroupType) | |
| GroupProperties | KeyValuePair | (Inherited from PubSubGroupType) | |
| Status | (Inherited from PubSubGroupType) |
Methods
AddDataSetReader
- BrowseName
- AddDataSetReader
| Name | DataType | Description |
|---|---|---|
| Configuration | DataSetReaderDataType |
| Name | DataType | Description |
|---|---|---|
| DataSetReaderNodeId | NodeId |
RemoveDataSetReader
- BrowseName
- RemoveDataSetReader
| Name | DataType | Description |
|---|---|---|
| DataSetReaderNodeId | NodeId |