PubSubCapabilitiesType
- BrowseName
- PubSubCapabilitiesType
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| MaxPubSubConnections | UInt32 | ||
| MaxWriterGroups | UInt32 | ||
| MaxReaderGroups | UInt32 | ||
| MaxDataSetWriters | UInt32 | ||
| MaxDataSetReaders | UInt32 | ||
| MaxFieldsPerDataSet | UInt32 | ||
| MaxDataSetWritersPerGroup | UInt32 | ||
| MaxNetworkMessageSizeDatagram | UInt32 | ||
| MaxNetworkMessageSizeBroker | UInt32 | ||
| SupportSecurityKeyPull | Boolean | ||
| SupportSecurityKeyPush | Boolean |