OperationLimitsType
- BrowseName
- OperationLimitsType
- SuperType
- Folder(FolderType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| MaxNodesPerRead | UInt32 | ||
| MaxNodesPerHistoryReadData | UInt32 | ||
| MaxNodesPerHistoryReadEvents | UInt32 | ||
| MaxNodesPerWrite | UInt32 | ||
| MaxNodesPerHistoryUpdateData | UInt32 | ||
| MaxNodesPerHistoryUpdateEvents | UInt32 | ||
| MaxNodesPerMethodCall | UInt32 | ||
| MaxNodesPerBrowse | UInt32 | ||
| MaxNodesPerRegisterNodes | UInt32 | ||
| MaxNodesPerTranslateBrowsePathsToNodeIds | UInt32 | ||
| MaxNodesPerNodeManagement | UInt32 | ||
| MaxMonitoredItemsPerCall | UInt32 |