ServerCapabilitiesType

BrowseName
ServerCapabilitiesType
SuperType
Object(BaseObjectType)

Properties

Name BrowseName DataType Description
ServerProfileArray String
LocaleIdArray LocaleId
MinSupportedSampleRate Duration
MaxBrowseContinuationPoints UInt16
MaxQueryContinuationPoints UInt16
MaxHistoryContinuationPoints UInt16
SoftwareCertificates SignedSoftwareCertificate
MaxArrayLength UInt32
MaxStringLength UInt32
MaxByteStringLength UInt32
<VendorCapability> BaseDataType
MaxSessions UInt32
MaxSubscriptions UInt32
MaxMonitoredItems UInt32
MaxSubscriptionsPerSession UInt32
MaxMonitoredItemsPerSubscription UInt32
MaxSelectClauseParameters UInt32
MaxWhereClauseParameters UInt32
MaxMonitoredItemsQueueSize UInt32
ConformanceUnits QualifiedName
OperationLimits OperationLimitsType
ModellingRules Folder
AggregateFunctions Folder
RoleSet