HistoryServerCapabilitiesType
- BrowseName
- HistoryServerCapabilitiesType
- SuperType
- Object(BaseObjectType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| AccessHistoryDataCapability | Boolean | ||
| AccessHistoryEventsCapability | Boolean | ||
| MaxReturnDataValues | UInt32 | ||
| MaxReturnEventValues | UInt32 | ||
| InsertDataCapability | Boolean | ||
| ReplaceDataCapability | Boolean | ||
| UpdateDataCapability | Boolean | ||
| DeleteRawCapability | Boolean | ||
| DeleteAtTimeCapability | Boolean | ||
| InsertEventCapability | Boolean | ||
| ReplaceEventCapability | Boolean | ||
| UpdateEventCapability | Boolean | ||
| DeleteEventCapability | Boolean | ||
| InsertAnnotationCapability | Boolean | ||
| ServerTimestampSupported | Boolean | ||
| AggregateFunctions | Folder |