ProgramStateMachineType
- BrowseName
- ProgramStateMachineType
- SuperType
- FiniteStateMachineType(FiniteStateMachineType)
Properties
| Name | BrowseName | DataType | Description |
|---|---|---|---|
| CurrentState | LocalizedText | ||
| LastTransition | LocalizedText | ||
| Creatable | Boolean | ||
| Deletable | Boolean | ||
| AutoDelete | Boolean | ||
| RecycleCount | Int32 | ||
| InstanceCount | UInt32 | ||
| MaxInstanceCount | UInt32 | ||
| MaxRecycleCount | UInt32 | ||
| ProgramDiagnostic | ProgramDiagnostic2DataType | ||
| FinalResultData | Object | ||
| Halted | |||
| Ready | |||
| Running | |||
| Suspended | |||
| HaltedToReady | |||
| ReadyToRunning | |||
| RunningToHalted | |||
| RunningToReady | |||
| RunningToSuspended | |||
| SuspendedToRunning | |||
| SuspendedToHalted | |||
| SuspendedToReady | |||
| ReadyToHalted | |||
| AvailableStates | NodeId | (Inherited from FiniteStateMachineType) | |
| AvailableTransitions | NodeId | (Inherited from FiniteStateMachineType) |
Methods
Start
- BrowseName
- Start
Suspend
- BrowseName
- Suspend
Resume
- BrowseName
- Resume
Halt
- BrowseName
- Halt
Reset
- BrowseName
- Reset